Skip navigation

News

Top & Trending
rezfo
It happens I have an HP8753c vna and a HP85060c ecal system. Unfortunately the 8753 firmware is version 4.01 and HP85060c wants 4.02 to control the analyzer. Someone knows if a patch exists to overcome this limit, or I have to continue using mechanical calibration with this VNA?
1

benalcazardiego
Hello. I am new to this device. I am using a E5071C ENA (2ports) with an external BIAS from a SMU which sweeps voltages for each frecuency. I want to confirm that the synchronization is done right and therefore I want to see the input signal that is applied on the DUT in the time domain. Can I do this connecting an oscilloscope? I expect to
2