Skip navigation

News

Top & Trending
rok
Hello Keysight,   I'm using the win7 PNA-X with A.10.49.11 firmware, which has both the Opt 28 and Opt 29 noise figure capabilities. I am trying to configure an opt 28 noise figure channel (i.e. use 'NA Receiver'). When I performed the calibration, I select 'Scalar' which grays out the rest of the available options. Then I perform a power
4

Soren_Marodoren
Hi,   I have an DSO-X 3024A without any installed licenses. But when I look in the About This Oscilloscope I see that BW20 is installed. What is that?   Best regards, /Sören
2