Skip navigation

News

Top & Trending
minolta1
Hello please where is possible to find or who has got firmware to spectrum analyzer HP 8591A (old version) ? I need U6 U7 U23 U24 and there are 27C512 eprom s. Labeled is 08590-80154 900103  (1990 year).or another version about 1990-91?  In this older type of CPU board is not possible to install 27C010 eproms with newer firmware (PAL
0

AdamCooman
Hello   I use the MatlabOutput command a lot in ADS to allow processing of the simulation data in Matlab. Recently I installed ADS2016.01. It is a really nice release, I enjoy the customising of the annotation a lot. But I noticed that the .mat files generated by ADS2016.01 are corrupt.   To verify that it was not my fault, I ran the
2
Top & Trending
Pat Harper
I saw a recent LinkedIn study that says most millennials who graduate from college this year will work for four different companies in the first decade of their career. I’m guessing my MBA students are amused when I tell them that early in my career, many engineers not only worked for a single employer for ten years, we sometimes worked on a
1
Top & Trending
mori001
Hi, I have 3 of this family scopes, one 54825A that is working fine, one scrap 54820A I use for parts and the other 54825A that has recently failed, the latter one displays a "Fine interpolator gain cal failed: Service is required" error and does not pass self test. This scope showed the same error 4-5 years ago and I replaced A/D part 1NB7-8353
0