Skip navigation

News

Top & Trending
Nutzer2016
Which is max. readout frequency for current draw measurements ?   GPIB interface is currently used. Port 0..25 V was used. I experienced approx. 4 current draw values per second as max readout frequency via GPIB. Is this documented somewhere ? I did not yet found this in the 'User's manual' .
1

Frank_BR
Most low and medium cost SA’s (spectrum analyzers) have a lower frequency limit equal to 100 kHz, or so. It is the case of my N1996A. Sometimes you need to analyze audio frequencies and it is good to know that it is possible to use such SA’s for the task. The “secret” is to
2
Top & Trending
AntonioLitterio
Good morning, I have a question on the N8736A power supply. We have one and we program it via Analog signal. We noticed that the OVP protection triggers without measuring with an oscilloscope a voltage at the output. Is it possible that if OVP protection is programmed at 40V and we apply an analog signal that should drive the PS output over
0
Top & Trending
LNegron0313
Hello,   I recently acquired an old 8561B w/ prefix 3017A. Powers on and completes the self tests but with errors 301 317 and 334 (suspect a dead YTO which is a common and costly issue or hopefully a dead LODA).   Currently I've been going over the 8561/3 E/EC manual as a general reference. I was wondering if anyone here or out there
1