Skip navigation


Top & Trending
USB Type-C connections bring you high-speed data rates, support multiple protocols and much more power than USB 3.0. Quickly see how the USB Type-C benefits will expand your electronics connectivity.    Create a Faster Path to Done USB Type-C Design and Test Learn more about USB Type-C at Keysight

I have written a program in C# that controls an Agilent 34970A with a 34901A MUX card installed. I can channels 101-119, import the values, and display them. I connect to the instrument through a serial connection. I started off using IVI-COM drivers, but I have found them to cause issues, so I have switched to the lower level SCPI drivers. I got