Skip navigation

News

Top & Trending
zhan3068
In the data sheet, the reading rate is  "5,000 rdgs/s std" . Is it for all the measurements, including resistance, capacitance, period? If yes, does that mean, even if different capacitance range is select, ex. 10nf and 10uf, the reading rates are the same?
1

Johann Glaser
Hi!   The integrated waveform generator (license DSOX3WAVEGEN) on my MSO-X 3024A behaves strangely. When generating a "Pulse" waveform and adjusting the frequency or the pulse width, the generated signal wildly jumps around. I would expect that the waveform steadily follows while I'm turning the knob.   Please see the attached scope
1
Top & Trending
HD
Hello All,   I have a complete RF test program developed in VEE. Now this test program is going to be used on a test computer to test a product. My problem is that there needs to be a wrapper around this program which calls the VEE test program and also controls a handler which changes the DUT. There is a need for handshake between the test
0