Skip navigation

News

Top & Trending
Faruk
Can I run vee pro on a tablet computer? The Tablet PC has a Windows operating system. Is Anybody try? Does have an idea?
1

Henry.B
Hello, i have a few problems with RFIC Dynamic Link on ADS Version 2015.01. I tried to do the "Getting Started with RFIC Dynamic Link" tutorial but it does not work. First of all i set up the Examples Directory as described and sourced setCSF.csh. I started the Cadence Virtuoso Design Environment and choosed "File > Open" from the Cadence
0
Top & Trending
circuit_maker
Hi, I am trying to simulate a structure as below:   I have to attach an SMD diode between ports, P1 and P2. I have SPICE model for the diode and C2 and L2 model the package, whereas L3 is for DC path. Separtion between P1 and P2 is 45mils whereas the pad size is 80mil/40mil. Now, If I define port P1 and P2 as TML, the EM cosimulated
2