Skip navigation

News

Top & Trending
Nutzer2016
Which is max. readout frequency for current draw measurements ?   GPIB interface is currently used. Port 0..25 V was used. I experienced approx. 4 current draw values per second as max readout frequency via GPIB. Is this documented somewhere ? I did not yet found this in the 'User's manual' .
1

Jiaru
Hello The problem is as showed below, when I open my libries. But few days before it works, same setting without any change.
9
Top & Trending
ravenn
hi, first, this is the first time i'm working with all of this... i am trying to read measured values from a 3458a multimeter. I'm working with excell and VBA and i managed to get readings into excell sheets, however i can't figure out how to get one reading at a time along with the time at which it was taken. Currently i can get one set of
0