Skip navigation

News

Top & Trending
rok
Hello Keysight,   I'm using the win7 PNA-X with A.10.49.11 firmware, which has both the Opt 28 and Opt 29 noise figure capabilities. I am trying to configure an opt 28 noise figure channel (i.e. use 'NA Receiver'). When I performed the calibration, I select 'Scalar' which grays out the rest of the available options. Then I perform a power
2

teddytoons
I've managed to get LABview to retrieve a PNA screen dump ( HCOPY:SDUMp:DATA?) and parsed the header info off of the PNG file, however, after saving the file, when I try to open it in Windows, I get an error saying the file is not the right format. I'm sure someone out there has successfully saved a PNA screen dump. (?) Below are two
12
Top & Trending
n12i
Hi I hope this is the right forum. I have a N6705B power generator and I am trying to use pyvisa to communicate with it. I wan to try to read in the voltage and current at the same time. I read that the power generator is able to interleave data, but is not able to read both at the same time. How would I do this? I tried to find some example
0