Skip navigation

News

Top & Trending
RrnR
I an in the process of replacing a 34401a with a 34410a in an ATE system.   The 34401a was controlled via RS232, but the 34410a doesn't offer that option, so the PC is running the VISA interface software and I am talking to the meter over a TCP/IP network.  It's pretty much going but for one thing:   With RS232 comms it was
4

Top & Trending
LNegron0313
Hello,   I recently acquired an old 8561B w/ prefix 3017A. Powers on and completes the self tests but with errors 301 317 and 334 (suspect a dead YTO which is a common and costly issue or hopefully a dead LODA).   Currently I've been going over the 8561/3 E/EC manual as a general reference. I was wondering if anyone here or out there
1