Skip navigation

News

Top & Trending
JohnPi
I am trying to do simultaneous measurements with two 34401A's over GPIB. Each is setup identically (10V, no autozero, no qutorange, 0.02 NPLC, 4 digit resolution), and I am using GPIB (BUS) triggering (with a trigger delay of 2 ms). I am using 10 samples, but that doesn't affect the issue. The two meters are identical except for firmware: one
5

rab82001
Hi   I'm new to VEE. I have inherited an application that was written using HP-VEE 5.01.  We're currently upgrading the OS and computer to Windows 7 and are planning to use VEE 9.32.  Will the old VEE program work out of the box with the new VEE software?  Are there any known pitfalls that I should watch for when transitioning
2
Top & Trending
jive-admin
Corporate Blogs Product Blogs Technology Blogs Insights Unlocked Digitizer Blog Automotive and Energy Solutions General Electronics Measurement Better Measurements: The RF Test Blog Keysight Services EEsof EDA Oscilloscopes Blog EEs Talk Tech Engineers Blog (Japanese)   Internet Infrastructure Next Generation Wireless
0
Top & Trending
chard
Can you provide more details on how the Unknown Thru Calibration works on the E5071C and how to apply it? The on-line manual does not describe the theory-of-operation or use-model. Here are some questions: 1) Is the Unknown-Thru method a modification to the cal kit? Is this just a correction method for the standard thru which I presume is a
3