Skip navigation

News

Top & Trending
jeffro
I was "tuning" a design and ADS froze during the session (ADS2014C linux).    Now the library I was working with can not be saved because it is stuck in "read only" mode.   From the ADS main window,  I went into Manage Libraries menu pick then selected the locked library and then  clicked on the pulldown "Change Library
1

hognala
Thought I would share how to install VEE 8.5 or 9 on Windows Vista/7 64-bit. VEE 8.5 / 9.0 will still run as a 32-bit app but that is ok. These are my observations and are not necessarily supported by Agilent. [list=1:3mo9gbnl]Step 1: Install IO Libraries Suite 15.5.13009.1  (released 14October, 2009 at 4:00 PM MST) from
3