Skip navigation

News

Top & Trending
Dr_Frank
The max. voltage rating for 3446xA and 34470A was changed in the specification recently, downgraded to 600V DC / 440V AC only.   What's the reason behind? Can I still use the full 1000V DC or 750V AC, as imprinted on my 1 1/2 years old 34465A? Will Keysight fix all units, to bring them to full specification again?   Frank
0

tamourjaved
Hello,    I have a 53220A counter/timer, I want to measure the time interval between two channels, the way I want it to work is that the the channel1 should wait for a particular trigger than start the timer and when a particular trigger is reached at channel 2 the timer stops and also the counter stops i.e I need only one time interval
12