Skip navigation

News

Top & Trending
LNegron0313
Hello,   I recently acquired an old 8561B w/ prefix 3017A. Powers on and completes the self tests but with errors 301 317 and 334 (suspect a dead YTO which is a common and costly issue or hopefully a dead LODA).   Currently I've been going over the 8561/3 E/EC manual as a general reference. I was wondering if anyone here or out there
1

Nutzer2016
Which is max. readout frequency for current draw measurements ?   GPIB interface is currently used. Port 0..25 V was used. I experienced approx. 4 current draw values per second as max readout frequency via GPIB. Is this documented somewhere ? I did not yet found this in the 'User's manual' .
1