Skip navigation

News

Top & Trending
benalcazardiego
Hello. I am new to this device. I am using a E5071C ENA (2ports) with an external BIAS from a SMU which sweeps voltages for each frecuency. I want to confirm that the synchronization is done right and therefore I want to see the input signal that is applied on the DUT in the time domain. Can I do this connecting an oscilloscope? I expect to
2

rezfo
It happens I have an HP8753c vna and a HP85060c ecal system. Unfortunately the 8753 firmware is version 4.01 and HP85060c wants 4.02 to control the analyzer. Someone knows if a patch exists to overcome this limit, or I have to continue using mechanical calibration with this VNA?
1
Top & Trending
JB001
Hi All, I am currently trying to use a N6752A to emulate a battery charger. This is a task that I often perform with the E3633A. The task involves forcing the supply into CC mode with a voltage and current limit. I use a source meter(in this case the N6785A) to sink the current. The idea is that the supply increases current until it hits the
2