Skip navigation


Top & Trending
I have been using a 34401A DVM very successfully in my VB6/VBA Software until recently.     For various reasons, I had to start using a test station computer with my software.  It is Windows XP 2000 SP3.  I still use VB6 and VBA to program test software.  The problem also occurs with the Agilent IO Connection Expert.

By Rachel Beddor The surge in low-speed serial buses in the consumer market has brought about the need for accurate protocol decoders. Traditionally, decoding a serial bus would mean a trip back to your introductory engineering class— lots of counting 1s and 0s. This method is tedious and prone to errors, so a better option is to use
Top & Trending
I would like to have the correct fan on-hand before taking the E4422B out of service for replacement.   The service guide only lists the large fan as p/n E4400-60062 and provides no other information.   I know it is a 12 Vdc fan but can anyone provide its dimensions, or better yet, a suitable vendor and part number? I would like to