Skip navigation

News

Top & Trending
johnniehancock
The Swiss Army™ knife of the test & measurement world is the oscilloscope. Not only can a scope be used to view time-domain waveforms (voltage vs time), which is the primary cutting blade of an oscilloscope, but many of today’s scopes have additional blades that can perform measurements that were formerly relegated to specialized
0

Duane Lowenstein
I have a friend who owns a classic old BMW. He loves that car. It’s fast, reliable, and fits him like a glove. It has plenty of bells and whistles—nothing like the newer models, of course, which are rolling data centers. But that’s part of the appeal. There are fewer parts to break. Except that now, when they do break, it’s
2
Top & Trending
HSLEE
EMPro Workshop provides various Lab examples to show the complete Electro-Magnetic (EM) simulation flow and the procedure from processes like solid modeling, simulation setup, simulations, data display, and post processing. These lab examples are based on FEM (Finite Element Method) and Finite Difference Time Domain (FDTD) simulation technologies.
0
Top & Trending
Lin_Ming_Chih
Key parameters of PCB materials, such as DK, TanD, dielectric height, etched trace width, copper thickness and roughness, are critical for high speed PCB transmission line design. In this mini workshop, Beatty series resonant impedance structures are used to improve accuracy of PCB material property extraction for EM simulation and signal
0