Skip navigation

News

Top & Trending
inception
Hey guys,   for our research team we need to have the opportunity to calibrate data offline, i.e. we want to read the error terms after a SOLT calibration off the E8364C PNA and calculate the correction by our own.   So far, we calibrate the PNA using a full 2-port SOLT calibration (with 85052B cal kit) and read the 12 error terms with
0

Kobi
I have a layout structure that implements GSG pads for transistor characterization. The GSG pad is connected to a co-planar transmission line that eventually connects to the device. Thus, I defined the Momentum ports as explicit ports where the Signal pad is the positive terminal of the port and the 2 ground pads are the negative terminals of the
5
Top & Trending
giofav
Hello, I need to import a Pspice model in ADS. The netlist contains voltage controlled sources where the output is defined via a table of values (ETABLE in Pspice), as a function of the input voltage. However, these sources cannot be read by ADS and I did not find any equivalent controlled source/look-up table in  ADS. How can I import
0