Skip navigation

News

Top & Trending
Andrew003
Hi Keysight,   We ran into an issue where the only available cal kit for the particular adapter we have to use does not cover the full frequency range we need to measure over. One suggestion I got the other day was to cal the VNA/cables with our Ecal, connect a M/F adapter pair together, measure the combo and halve the S2P data. I feel like
12

DavieK
Hi   Can the boundary scan tested developed for the N1125A x1149 be run from an external test executive either C based or National Instruments TestStand.
0