Skip navigation

News

Top & Trending
rraman64
Hai all, I have specific task of using the edge then edge trigger and store the wave forms for offline analysis. Have two time-correlated  random pulse trains into ch 1 & 2. I arm with ch1 and trigger  with edge then edge trigger mode on event 0. When I use quick save using multipurpose trigger task, I was expecting each set/file
8

Top & Trending
AntonioLitterio
Good morning, I have a question on the N8736A power supply. We have one and we program it via Analog signal. We noticed that the OVP protection triggers without measuring with an oscilloscope a voltage at the output. Is it possible that if OVP protection is programmed at 40V and we apply an analog signal that should drive the PS output over
0