Skip navigation

News

Top & Trending
hafrse
Hello,   Have a problem in my power supply , it suddenly started to kick  start every 1.5 sec , when I remove the power supply sockets from almost all the cards, it starts but with a  hiss sound,  checked the caps , no visible leakage . All the powers supplies green LED:s lights on the CPU card , they fade away and lights on
0

minolta1
Hello please where is possible to find or who has got firmware to spectrum analyzer HP 8591A (old version) ? I need U6 U7 U23 U24 and there are 27C512 eprom s. Labeled is 08590-80154 900103  (1990 year).or another version about 1990-91?  In this older type of CPU board is not possible to install 27C010 eproms with newer firmware (PAL
0
Top & Trending
rraman64
Hai all, I have specific task of using the edge then edge trigger and store the wave forms for offline analysis. Have two time-correlated  random pulse trains into ch 1 & 2. I arm with ch1 and trigger  with edge then edge trigger mode on event 0. When I use quick save using multipurpose trigger task, I was expecting each set/file
5