Skip navigation

News

Top & Trending
rok
Hello Keysight,   I'm using the win7 PNA-X with A.10.49.11 firmware, which has both the Opt 28 and Opt 29 noise figure capabilities. I am trying to configure an opt 28 noise figure channel (i.e. use 'NA Receiver'). When I performed the calibration, I select 'Scalar' which grays out the rest of the available options. Then I perform a power
4

Soren_Marodoren
Hi,   I have an DSO-X 3024A without any installed licenses. But when I look in the About This Oscilloscope I see that BW20 is installed. What is that?   Best regards, /Sören
2
Top & Trending
n12i
Hi I hope this is the right forum. I have a N6705B power generator and I am trying to use pyvisa to communicate with it. I wan to try to read in the voltage and current at the same time. I read that the power generator is able to interleave data, but is not able to read both at the same time. How would I do this? I tried to find some example
0