Skip navigation

News

Top & Trending
arunnaidu
I would like to substitute one of the timed filters used as a channel filter in an example system simulation with measured S2P of an actual filter. I've tried to use transient analysis in a subsheet to enable this, but I'm getting a lot of time step errors. Has anyone done this successfully?  
5

drkirkby
At the following link   N9923A-308 Vector Voltmeter | Keysight (formerly Agilent’s Electronic Measurement)    it says "FieldFox offers the key functionalities of the HP 8058A, in a handheld form-factor, and without the need for the bridge and accessories required with the HP 8058A.."  I find that a bit hard to
2