Skip navigation

News

Top & Trending
ErinEast
The second the probe is connected to your device your signal begins a grand journey to the center of the scope. It has to pass through five phases in order to complete its journey to the center, then back up to the surface. First the signal has to find its way to the front of the scope through the probe. Then, once it enters the scope, it has to
0

sujith.nair
Will the 83752B Synthesized Sweeper work as a source for 8510C? The 8510C Pre-Flight setup document only lists up to 8360 series and not the 8370 and hence not sure if its readily compatible with 8510C or weather there are significant hoops I need to jump over to get them to work. Any insight you have would help.   Thanks, Sujith
0
Top & Trending
ErinEast
Let’s be honest, oscilloscopes aren’t exactly something you can just pick up and use without some sort of help or prior experience. Typically, it takes a bit of time and practice to understand how to use one correctly and make accurate measurements. We don’t want you wasting time trying to figure out how to use your oscilloscope
0