Skip navigation

News

Top & Trending
Lin_Ming_Chih
Key parameters of PCB materials, such as DK, TanD, dielectric height, etched trace width, copper thickness and roughness, are critical for high speed PCB transmission line design. In this mini workshop, Beatty series resonant impedance structures are used to improve accuracy of PCB material property extraction for EM simulation and signal
0

Kobi
I have a layout structure that implements GSG pads for transistor characterization. The GSG pad is connected to a co-planar transmission line that eventually connects to the device. Thus, I defined the Momentum ports as explicit ports where the Signal pad is the positive terminal of the port and the 2 ground pads are the negative terminals of the
2