Skip navigation

News

Top & Trending
matthieu.e
Hi,   I bought a used DSOX2002A. I updated it to firmware 2.35 and I started the 30 days of evaluation. The scope functions are OK. On the demo PIN all the signals are OK but I can't use the waveform generator function.   When I switch on the scope I have the message "Too high a voltage is being applied to the waveform generator BNC".
0

AlexeyTelegin
Источники питания постоянного тока серии Keysight E36100 после проведения соответствующих технических испытаний включены в Госреестр СИ РФ за номером № 64742-16, приказ # 1079 от 12 августа 2016  Серия компактных источников питания постоянного тока Keysight E36100 с интерфейсами LAN и USB обеспечивает точное и надёжное питание для отладки и
0
Top & Trending
LNegron0313
Hello,   I recently acquired an old 8561B w/ prefix 3017A. Powers on and completes the self tests but with errors 301 317 and 334 (suspect a dead YTO which is a common and costly issue or hopefully a dead LODA).   Currently I've been going over the 8561/3 E/EC manual as a general reference. I was wondering if anyone here or out there
0
Top & Trending
cresis_help
Hello,   Whenever I try to run TLine in Genesys 2015.08, I receive the following error. I just installed the software, and there is no Default.eg$ anywhere in my program files. I am using Windows 7 and have had other people try it on their computers, but they receive the same error.    Any help is much appreciated and let me
0
Top & Trending
Pat Harper
I saw a recent LinkedIn study that says most millennials who graduate from college this year will work for four different companies in the first decade of their career. I’m guessing my MBA students are amused when I tell them that early in my career, many engineers not only worked for a single employer for ten years, we sometimes worked on a
1