Skip navigation


Top & Trending
I have been using a 34401A DVM very successfully in my VB6/VBA Software until recently.     For various reasons, I had to start using a test station computer with my software.  It is Windows XP 2000 SP3.  I still use VB6 and VBA to program test software.  The problem also occurs with the Agilent IO Connection Expert.

I need information Analyzer Spectrum N9020A about PEAK TABLE, I have five result that I get. I'm used following comand: CALC:MARK:PEAK:THR:STAT ON CALC:MARK:PEAK:THR -12 dBm CALC:MARK:PEAK:EXC 8 dB CALC:MARK:PEAK:TABL:STAT ON CALC:MARK:PEAK:TABL:READ GTDL   How to get result PEAK TABLE listed in the table with command SCSI?