Skip navigation

News

Top & Trending
solid
Is there any way to concatenate SCPI commands in test flow? when i try i get "Cannot concatenate two SCPI commands in one step". However, i have equipment that needs *WAI command concatenated to measurement queries to hold the GPIB bus while the measurements are made!
11

bar28
My guestion is rather basic, but still important when doing mecahnical calibrations. When using mechanical 2.4mm 85056D calibration kit, what is most right way to make connection? Especially when connecting male standards to 85130G female-NMD connector.  Always has teached, that body of the standard must keep steady when doing mating. Well,
0