Skip navigation

News

Top & Trending
rraman64
Hai all, I have specific task of using the edge then edge trigger and store the wave forms for offline analysis. Have two time-correlated  random pulse trains into ch 1 & 2. I arm with ch1 and trigger  with edge then edge trigger mode on event 0. When I use quick save using multipurpose trigger task, I was expecting each set/file
3

bmacs
I have successfully used TCM working with the Freescale LTE PHY chipset.  So far, I have been unsuccessful using TCM with the Intel (Mindspeed) PHY.
1