Skip navigation

News

Top & Trending
bowilzhang‘’
It is well known that the error model of the SMC algorithm has been expressed by the signal flow diagram, what is the error model of the X parameter (signal flow diagram)?Is it possible to provide relevant reference materials?
2

tp78
I have the ADS/Python link working. End goal is to try run a simple envelope simulation, take the signal and pass it into python, perform some signal processing, and then return to ADS. I ran into issues that can be summarized by the attached description. Basically for different array lengths the shape of the returned data varies.  
0
Top & Trending
adamsussex
I am trying to set up dynamic sequencing on my M8190A AWG. I am controlling the AWG via a C++ program which calculates the waveforms and sends the necessary commands to the AWG to upload the data. This program works for single segments but so far I have been having trouble getting it to work for sequences. I am able to define a sequence via the
0