Skip navigation

News

Top & Trending
rok
Hello Keysight,   I'm using the win7 PNA-X with A.10.49.11 firmware, which has both the Opt 28 and Opt 29 noise figure capabilities. I am trying to configure an opt 28 noise figure channel (i.e. use 'NA Receiver'). When I performed the calibration, I select 'Scalar' which grays out the rest of the available options. Then I perform a power
4

surfer113
When i save data from osciloscope I want the values from logic analizer to be save in binary and not HEX format. Can someone tell me how to do this? Thanks
1