Skip navigation

News

Top & Trending
Dr_Frank
The max. voltage rating for 3446xA and 34470A was changed in the specification recently, downgraded to 600V DC / 440V AC only.   What's the reason behind? Can I still use the full 1000V DC or 750V AC, as imprinted on my 1 1/2 years old 34465A? Will Keysight fix all units, to bring them to full specification again?   Frank
0

simon_coleby
[vrf] VEEOS R1 ready for Users   Hi All   I'm pleased to announce that I finally found some time and the first real release of the VEEOS library is now ready for use. Wander by veeos.org and go at it!   This is fully compatible with the last trial releases but now has full documentation and many areas that have been cleaned up.
0