stmichel

Webcast - Advanced Techniques for Validating PCI Express® 4.0 Transmitters and Receivers

Blog Post created by stmichel Employee on Jan 8, 2018

With demand on networking and computer performance increasing at a rapid pace, there is a growing need to store, move and process more data in real-time than ever before. As data speeds increase, channel attenuation becomes an inhibitor to moving data across an interface bus. This webcast will highlight Keysight’s contributions with PCIe® 4.0 technology for physical layer transmitter and receiver testing. Topics will include improvements to the PCI Express 3.0 CEM connector to support 16 GT/s signaling, improvements to receiver testing methodologies for paving the way to PCI Express 4.0.

 

Join Keysight’s Rick Eads , an active contributor within the PCI-SIG workgroup, for a 1-hour webcast  on January 17  to learn more about:

  • The key challenges of developing a #PCIe 4.0 link capable of 16GT/s operation
  • The changes to the channel and connector interface that are needed
  • The tools available to help characterize and debug PCIe 4.0 transmitters and receivers

 

  Rick Eads - Keysight's active contributor  to the PCI-SIG workgroup   Join Webcast.

If you don't see the webcast in the list, click onSelect Country and select 'US'.

Outcomes