In my previous post, I showed you the "all-in-one" method for adding your Verilog-A models to ADS. In this post, I'll show you another method called "shared library." It's a bit more work to set up, but it saves time in the long run because it avoids duplication of effort in each new project. If you give a project workspace to a colleague you have to remember to give the referenced library also. In fact, this shared library method is just good not only for Verilog-A components but also for component models of other types (e.g. netlist-based models/model cards). It's a good method anytime you have component models that are common to several projects. Like last time, there are quite a few steps, but each one is really easy.
Shared Library
- Follow steps 1 through 20 of Part 2, except this time, in step 2, name the workspace something like shared_wrk. Alternatively, make a copy of all_in1_wrk, rename it shared_wrk, and then delete the testbench cell.
- In the Main window, select the Library View tab. When you created the workspace, ADS automatically created a default library under it. The default name is created by replacing the _wrk suffix with a _lib suffix. So in our case it is called shared_lib. Right click on the library and select Configure Library... from the popup context menu.
- In the Library Configuration Editor, Simulation tab, click on the Browse... button to the right of the Verilog-A directory edit box. Browse up one level and select the veriloga folder. Alternatively, you can just type ..\veriloga into the edit box. The relative path-name is preferred over an absolute path because if you give the library to a colleague, they might install it with different root name. Dismiss the Library Configuration Editor by clicking on the OK button. It reminds you that changes will take effect next time you open it. Click OK.
- From the main window menu bar, select File-->Close Workspace. We are done with the shared library for now. Let's imagine we are starting the first of several projects that will refer to the shared library.
- From the ADS Main Window menu bar, select File-->New-->Workspace...
- From the New Workspace dialog box, give it a name like project1_wrk and then click the Create Workspace button.
- From the Main window menu bar, select File-->Manage Libraries...
- From the Manage Libraries dialog box, click on the "Add Library Definition File..." button.
- From the Select Library Definition File browser, navigate to the previous workspace (i.e. your shared_wrk folder) and locate and select a file called lib.defs then click the Open button.
- Dismiss the Manage Libraries dialog box by clicking on the Close button.
- In the Main window Folder View tab, click on the little arrow by the resistor cell folder. You should see the symbol view of the cell.
- From the Main window menu bar, select File-->New-->Schematic... and name its cell something like testbench.
- Create Arrange the Main window and the new testbench schematic window side-by-side.
- Click and drag the resistor symbol from the Main window to the testbench schematic window. Instantiate your resistor by clicking anywhere on the schematic canvas. Set it to 2 ohms.
- Create a simple testbench like this:
- Click on the Simulate icon or select Simulate-->Simulate or just hit the F7 shortcut key. The first time you simulate, there is a short pause while ADS compiles the Verilog code. It saves the compiled model, so if you don't touch the code, there is no need to re-compile the next time you run it.
- From the Data Display window, insert a plot, and select the Vout and branch current (_ub_p_n_i) traces:
I added some markers and played around with the axis and trace settings.
Success! Now you create project_2, project_3 and so on. Repeat steps 5-17 for each new project to refer to your shared library thus reusing it.
In the next posting, we'll return to the main topic: how to translate the analog parts of VHDL-AMS to Verilog-A. Part 1 was a resistor. Part 4 is a comparison of how the two languages handle time derivatives and internal branches.