Keysight EEsof EDA’s Advanced Design System (ADS) software can help you overcome your signal and power integrity challenges. As the world’s leading electronic design automation for RF/MW and high-speed digital applications, ADS features a host of new technologies designed to improve productivity, including two EM software solutions specifically created to help signal and power integrity engineers improve high-speed link performance in PCB designs.
Below are ten ways ADS can solve your most common SI/PI Design Challenges.
1. ADS provides speed and accuracy for your SI EM characterization
Don't be slowed down by increasing data rates. ADS provides two EM analysis solutions - SIPro and PIPro - that are specifically designed to handle high data rates, without sacrificing accuracy or speed. The limiting factor of 3D-EM technology for SI analysis is simply the scale and complexity of PCB designs. However, SIPro focuses on enabling SI EM analysis of high-speed links on large, complex high-speed PCBs, while PIPro is used for PI EM analysis of power distribution networks, including DC IR drop analysis, AC PDN impedance analysis, and power plane resonance analysis.
Figure 1. SIPro delivers results approaching the accuracy of full-wave 3D-EM solutions, but in a fraction of the time.
2. ADS simplifies the use of S-parameter files for your parts
Imagine you’ve just downloaded an S-parameter file for a part you are considering; in this case, a high-speed connector for a backplane. It has a large number of ports on it, so you want to first inspect the quality of the data and then use it in your simulation. How do you wire it up? Which ports are paired?
Traditionally, the answer might be to open up the data in a text editor. However, with ADS’s S-Parameter Checker, designers can now easily view the contents of any S-parameter file without having to setup an S-parameter test bench simulation. This allows them to directly plot the individual relations they wish to see, and shows them the port names against each pin. It also tells designers if the file is passive or reciprocal, as well as the number of data points in the file and the frequency range it covers. Designers can even use S-Parameter Checker to rename, re-order and reduce the number of ports, which enables them to save a new, more usable S-parameter file (Figure 2).
Figure 2. The S-Parameter Checker allows design engineers to easily rename, re-order and reduce the number of ports.
3. ADS provides access to industry-leading channel simulator technology
ADS's channel simulator technology sprung forth in 2009 when transient simulation (SPICE) couldn’t address the measurement of margin-to-mask for really low bit-error-rates (BER), as demanded by high-speed link designs.
Dr. Fangyi Rao's 2006 patent to correct for passivity, while ensuring causality, ensured ADS to be regarded as the msot accurate solution for handling cascades of S-parameter models combined with circuit models in one schematic. The pace of innovation continues today with ADS's Channel Simulator still the industry-standard model. Additionally, the Channel Simulator now supports IBIS package (.pkg) entries directly and more extensively before.
Figure 3. With ADS, designers can mix-and-match models from IBIS, IBIS-AMI, SPICE, and generic built-in models.
4. ADS stays ahead of technology waves (such as PAM-4)
Market pressures on IP routers set an expectation to do more at a lower cost per bit. However, to go faster and provide a single 100-Gbps electrical lane across the distance of a typical backpane is beyond present day technology.
The solution lies in Pulsed-Amplitude Modulation (PAM) for high speed serial links. PAM represents a revolutionary step in the industry, but comes with its own unique set of challenges as well. For example, we can transmit a PAM-4 symbol at 28 Gbaud and deliver 56 Gbps at the other end, but the IC's use more power and the signal itself has a reduced Signal-to-Noise ratio (SNR).
Whether you are challenged with managing complexity while reducing production cost, or researching how to go further and faster on low-loss materials and fabrication processes,
Figure 4. ADS supports PAM-4 simulations, which offers a viable alternative to NRZ.
5. ADS accelerates DDR4 simulation methodologies
In simulations, how do you check compliance against the mask? Keysight EDA offers a novel DDR Bus simulator specifically designed to accomplish this task. It is a bit-by-bit channel simulator for parallel buses. It characterizes all transmitter paths at once, and calculates the BER contours for each eye at the receive side, together with the measurements for margin to mask.
The simulator is unique in that it correctly handles the asymmetric rise and falling edges found with single-ended signals.The Tx and Rx models can be used to drive IBIS models, or mixed with SPICE models. The speed of the simulator allows it to be used in place to transient simulation for many pre-layout tasks, where the designer wants to sweep multiple parameters, or investigate performance movements. Together with batch simulation, it is a powerful tool for pre-layout design exploration, as well as post-layout verification for compliance.
Figure 5. Keysight EEsof EDA's DDR Bus simulator is a bit-by-bit channel simulator for parallel buses.
6. ADS puts power in the hands of designers
Power Integrity has become an ever-increasing challenge in modern day high-speed systems, driven by three main forces: higher device integration, lower IC supply voltages, and smaller real estate on the PCB. These modern challenges have forced engineers out of their notebooks and into true PI-DC simulators in order to take into account the real physical layout of the power delivery network (PDN).
With ADS and the new PIPro suite of EM simulators, designers receive visual feedback in just second on exactly what the voltage distribution looks like for the selected power and ground nets. ADS also allows designers to check the current flow through individual vias and the voltage and current at specific locations like individual pins on the sinks and voltage regulator module (VRM). This information is easily reported in a sortable table. Vias that carry too much current can be highlighted in the layout for easy identification (Figure 6).
Figure 6. Vias carrying too much current can be highlighted in the layout for easy identification.
7. ADS enables flat PDN impedance responses
Once the initial pre-layout design has been created, the first-pass of the PCB layout can be imported into ADS 2016 for analysis using PIPro EM technology. PIPro’s net-driven user interface allows designers to quickly select the power and ground nets for the PDN network they want to simulate, choose simulation models for each of the components (e.g., decaps, EMI filters, inductors, and resistors, etc.), and setup the PI-AC simulator to compute the PDN impedance of the distributed layout with components in place.
Since the PI-AC simulator has EM technology designed specifically for this purpose, a very accurate result is returned in minutes, not days. Designers can then use ADS 2016’s field visualization, PDN impedance and S-parameter plotting to determine if there are problems with the current PDN design, and to check coupling from one capacitor to the next. With just one click, a schematic representation is generated to transfer the EM-characterized model, together with circuit models of the components. This back-annotation to an ADS Schematic enables one smooth cohesive workflow. Designers can then apply their behavioral VRM model, and further tune the decaps for final verification/optimization.
Figure 7. Increasing the decoupling capacitance while increasing ESR improves impedance response flatness.
8. ADS enables electro-thermal simulation
As power delivery networks are forced into tighter PCB real-estate, the power plane becomes far from idealized. Usually the once perfect plane is perforated heavily with clearance holes from stitching vias, and it can be a struggle for the layout engineer to get the required current up into the package of the device that requires it, without passing through narrow traces of metal. Calculating an accurate IR-Drop is important for the PI designer, but also knowing the absolute temperature that the PDN traces, vias and chip die will reach, is invaluable information. High temperatures can cause reliability issues; as the temperature cycles from on/off states can cause the via barrels to weaken and crack over time.
It is not intuitive to the designer whether a via is undersized for the current that is passing through it. The temperature rise is very dependent on the width of the traces attached to it. Secondly, resistance of a trace increases with temperature, requiring simulation analyses to determine the final steady state condition. For every 10 degC change in temperature we see a 4% change in resistance of a trace. These observations point to a need to simulate the PDN design with a DC IR Drop electro-thermal solution.
ADS provides a fully-automated integrated Electrical-Thermal-Electrical iterative simulation. Users receive the most accurate representation of DC IR Drop results by taking into account local resistivity changes due to heating. The additional Thermal-only simulation, gives the user the ability to perform thermal floor planning.
With ADS you can easily copy existing DC IR Drop simulation setup to new Electro-Thermal simulation and visualize a list the temperature of planes, pins and vias.
Figure 8. DC IR Drop Electro-Thermal analysis - visualization of temperature.
9. ADS has an interconnect toolbox (Via Designer and CILD)
The signal integrity design challenge is not just to successfully recover the transmitter signal at the receiver, but to understand what is controlling the performance. What are the significant margin eaters and which ones can I optimize?
Typical connections between a transmitter and a receiver include some section of application specific custom PCB routing. ADS has a signal integrity tool box to help explore the design trade-offs and deal with the complex interaction between stack-up, transmission line losses, and via topology.
Designing the PCB interconnect starts with some sort of PCB stack-up definition in order to start evaluating the different types of possible transmission line topologies. Once the transmission lines are optimized for impedance and losses, then one needs to look at via performance to transition between layers. Anyone of these steps has cost and performance trade-offs that can impact the other, resulting in a complex inter-relationship to determine which feature is the real margin eater: Layer Count, Line Z, Via Backdrills, Material, Layout Density, etc.
ADS provides an Interconnect Tool Box that includes Substrate Editor, Controlled Impedance Line Designer, and Via Designer to simplify the pre-layout PCB interconnect investigation.
Figure 9. This type of pre-layout investigation enables an engineer to understand what is controlling the design margins and make informed cost vs. performance decisions.
10. ADS embodies the Keysight philosophy:
Hardware + Software + People = Insights
With Keysight's greater software-centric solutions focus, Keysight EEsof EDA plays a leading role in virtual compliance testing. Through Compliance Test Benches in ADS, designers can now take ADS simulated waveforms and test them against the same gold suite of compliance tests used on the bench with final verification hardware to attain the utmost confidence in a designs's compliance.
Further bolstering these capabilities in ADS is the support Keysight EDA offers its customers. That support includes a world-wide technical support presence, expert Application Engineers and consultative Field Sales Engineers. This support, together with Keysight’s hardware and software solutions and technical expertise gives customers greater insight and in turn, greater chance of success.
Keysight ADS further cements its leading position in electronic design software with continued advances for circuit simulation, layout and layout verification, silicon RFIC, and just as critically, signal and power integrity.