Skip navigation
All Places > Keysight Blogs > EEsof EDA > Blog > 2017 > October > 04

EEsof EDA

October 4, 2017 Previous day Next day

Signal and Power Integrity engineers look to ADS for the correct treatment of high-speed effects like distortion, mismatch, and cross-talk. Building on the strong foundation and loyal users ADS has amassed through the years, ADS 2017 delivers new options and functionality that enable it to be the tool today's designers need to get ahead.

 

The latest release of ADS is a stronger, faster, and more comprehensive platform for signal and power integrity analysis. Read about the top 10 new features in ADS 2017 for Signal and Power Integrity Engineers or watch the video.


 

10. Improved substrate editor

The new and improved substrate editor has an efficient edit feature for a larger number of layers. The simplified editor interface reduces simulation setup time and increases productivity.

ads2017 substrate editor

9. Fast Wire labeling

Labeling ports with the correct node names is time consuming, especially when you have many ports. With the new CSV import labeling, naming more than 10 ports is simple. 

ads2017 fast wire labeling

 

8. Parallel Sweep on windows

In ADS 2017, Batch simulation is able to run in Turbo mode in both Linux and windows. Using the 8-pack Element license and simulation manager, you can unleash the parallel computing power of your workstation PC. Reduce simulation time of large sweeps with simulation manager.

ads2017 parallel sweep

 

7. Statistical mode PAM -4

To simulate a PAM-4 signal down to 10 ^ -16 BER, a bit-by-bit simulation would take hours. ADS 2017 now supports PAM-4 in statistical mode. You can directly simulate PAM-4 to very low BER in a matter of seconds to minutes.

 

6. Mixed-mode S-parameter Checker

In the improved S-parameter checker, you can now convert single-ended S-parameters to mixed-mode in a few clicks. Save time and increase your productivity by letting the S-parameter checker show you the mixed-mode response.

ads2017 mixed mode s-param checker

 

5. S-parameter Spectral Thresholding

Usually, you would expect simulation speed to decrease with higher port count. In ADS 2017, the spectral thresholding algorithm removes weakly coupled ports before simulation. The result is faster simulation speed for a higher port count, without sacrificing accuracy.

ads2017 faster simulation

 

4. New and improved IBIS Components

Are you looking for specific pins in your IBIS model to interact with? The improved IBIS component interface helps you quickly sort and select desired pins. With built-in smart default settings, the IBIS schematic is cleaner, and setup time is faster.
ibis components

 

3. 3D Via Designer: Enabling Access to Accurate Via Models

A crucial problem when simulating high-speed signal interconnects is a lack of access to via models that are accurate at high frequencies. To solve this problem, ADS 2017 introduces Via Designer, a tool for creating and modeling PCB vias (single-ended or differential), while giving you full control over the via specifics.
ads2017 3d via designer

 

2. PIPro Bill of Materials Optimization for Decaps

Decap Optimization in PIPro can take all the decaps as laid out on the board, and search for the optimal solution that meets the desired target impedance profile. The user can define an optimal solution, by specifying weighted criteria such as: number of decaps, unique models, vendors, or cost. PIPro's algorithm intelligently ranks your best candidate solutions so you arrive at the best trade-off between performance and cost.

decap output

 

1. PIPro DC Electro-Thermal Capability

To find the true IR-drop of your power distribution network, thermal effects need to be considered in your analysis. PIPro performs an automated, iterative electric and thermal solve on each PDN, providing thermal insights to every power integrity engineer. PIPro calculates the temperature distribution of the board, so you can ensure the temperatures of vias, traces, and devices in your design are within the specification.  

ads2017 electro-thermal

 

 

These 10 new features are just the beginning of all the new capabilities and usability enhancements in the latest release of Advanced Design System (ADS) 2017. Along with improvements for the Signal and Power Integrity Designers are improvements for RF/MW designers doing RF front-end module and Silicon RFIC design. Check out all the new features on the web page and apply for your free trial of ADS 2017 today.

free trial of ADS 2017

FREE Evaluation of ADS | Keysight EEsof EDA