Skip navigation
All Places > Keysight Blogs > EEsof EDA > Blog > 2016 > December > 15

EEsof EDA

December 15, 2016 Previous day Next day

It’s a common problem. You’ve just downloaded the S-parameter file for a part you’re considering using in your design; say, a high-speed connector for a backplane. Because it has a large number of ports, the first thing you want to do is inspect the quality of the data. Then, you want to use it in your simulation. But, how exactly do you wire it up and which ports do you pair?

 

You can go the traditional route, which involves opening the data in a text editor. But given the overall complexity and time consuming nature of the design process in general, there has got to be an easier way to deal with this data. And now there is! It’s a feature called the S-Parameter Checker and it’s available in ADS 2016 (FREE trial available here).

 

With S-Parameter Checker, you can easily view S-parameter file contents without ever having to setup an S-parameter test bench simulation (Figure 1). Instead, you directly plot the individual relations you want to see. You can also see the port names against each pin. The software tells you whether the file is passive or reciprocal, as well as the number of data points in the file and the frequency range it covers.

ADS 2016, S-Parameter Files, Keysight EEsof EDA, S-Parameter Checker

Figure 1. ADS 2016 S-Parameter Checker allows design engineers to easily rename, re-order and reduce the number of ports, enabling a new, more usable S-parameter file.

 Keysight EEsof EDA, ADS 2016, Signal Integrity, Power Integrity, SnP Component

Figure 2. ADS 2016 SnP component reads port names from the file directly onto the symbol, and allows you to choose the pin orientation.

 

Using S-Parameter Checker isn’t the only way that using S-Parameter files in ADS 2016 is now easier than ever before.

 

With a new SnP component, port names can be read from the file directly onto the symbol for simulation (Figure 2). This leaves you free to choose the orientation of your pins so that all inputs are on one side and all outputs are on the other side—and that means no more crossing of wires. Once that step is accomplished, all you have to do is view, edit, place, simulate, and plot (Figure 3).

SIPro, PIPro, ADS 2016, S-Parameter Checker, SnP component, S-Parameter, Keysight EEsof EDA

Figure 3. Using S-Parameter Checker and SnP component, using an S-parameter file for a part is now easier than ever before.

 

For more information on overcoming this and other design challenges, check out 8 Ways ADS 2016 Helps You Overcome Signal and Power Integrity Challenges.

Apply for a free trial