It is often the case that our manually calculated values do not provide optimum performance. Tuning is a way to change the component values and see the impact on circuit performance. Optimization is an automated procedure of achieving the circuit performance in which ADS can modify the circuit component values in order to meet the specific optimization goals. Download the Tuning and Optimization chapter from the ADS Example Book.
Click HERE to download more chapters.