Skip navigation
All Places > Discussion Forums

Signal Studio Software

Log in to follow, share, and participate in this community.

Recent Activity

JE499
Hello: I have 30+ emitters at different frequencies and different PRI/PW/agility structures and scan/antenna patterns. I need to sequence them so that each gets emitted to some time pattern. I am creating these signals using MESG software. Which way is the best to create them? Or else are they the same? * Create one PDW using multiple emitters… (Show more)
in Signal Studio Software