• Verify MMEM:STOR created file correctly via USB

    I am connecting to an N9020B via the USB interface and running a Python script that does screen captures to a USB drive using the MMEM:STOR:SCR <filename> command. As far as I can tell, there is no way to copy t...
    evan_davis
    last modified by evan_davis
  • How to control E5052B using socket programming?

    Hi: I want to control E5052B from my arm board which is running linux. I use socket communication to send SCPI commands to port 5025. The communication can be established, but E5052B doesn't respond to the command. Ho...
    xiaosa_en
    last modified by xiaosa_en
  • N9010A: Recording a Marker when Avg|Hold = 100/100 using SCPI

    Hello,   Recently I have been automating tests with pyvisa and ran into this issue. When testing for average spectral density, I was wondering if I was missing a SCPI command that will allow me to find when the ...
    efloden
    last modified by efloden
  • how to set up occupied bandwidth on n9020

    how to set up occupied bandwidth on n9020
    JEFFS003
    last modified by JEFFS003
  • Use of multiple FFT analyzer (synchronization)

    Hallo, I'm posting here because it sounds the best place for this topic after all. My problem is the synchronization of two FFT analyzer (either 35670 or 3563, we have two of both) where one is primary and the other i...
    mariscotti
    last modified by mariscotti
  • ESA E4402B Processor nach "Clearing Flash EPROM" ohne Funktion

    Nach Tausch der Processor Batterie kam folgende Start-Fehlermeldung "LO Unlock und LO Unlevel", danach habe ich eine "Clearing Dynamic RAM" und "Clearing Flsah EPROM" gestartet. Anschließen ist nach Neustart mein...
    Laphroaig
    created by Laphroaig
  • ESA E4407B ticking sound trouble

    Hello, I recently got an ESA E4407B analyzer. From time to time I hear a faint creak or regular ticking from inside the unit. It happens at the end of (but not everyone's) sweep. To hear it more clearly, I changed the...
    TomasK
    last modified by TomasK
  • time constant of peak detector

    I am going through the test for DO-160.   In the emission part of it, it states that: "The time constant of the peak detector must be lower or equal to 1/BW."   I am using N9038A for now, and I am curious ...
    TshawS
    last modified by TshawS
  • 8565E service guide incomplete?

    Hello: Well, yes I found the service guide on a previous post...but all the Component Level Information Package (CLIPs) is missing?? Anyway it can be downloaded as a separate file....  
    martine1212
    last modified by martine1212
  • HP8563E YTO FM driver issue

    Hello,   My HP8563E (3305A00721) has had a YTO replacement. Now it is error free upon start-up and seems to work fine. However, if I look at the cal signal at 300 MHz and reduce Span from about 13.5 MHz to 6.8 M...
    Harke001
    last modified by Harke001
  • Can I control display brightness? The Windows control seems to have no effect.

    I need to reduce brightness to balance light for recording and the display is very bright compared to the grey color scheme. Is there a control to dim the display (not OFF, just dim with a few choices maybe 5% to 100%).
    Christopher Kelly
    last modified by Christopher Kelly
  • replace by hp8593e option 151 and 160  by option 102

    Hello everyone,   I wanna install option 102 in my spectrum analyzer hp8593e but the PCB bay is full. Because i think option 151 and 160 has no use for my non professional usage (something for telecom company's...
    pe2ben
    last modified by pe2ben
  • 89441A Calibration Software

    Greetings, At one time automated performance verification software was included with the 89441A. While I realize the instrument is no longer supported by Agilent - is this performance verification software available ...
    AKeith
    last modified by AKeith
  • N9320B USB failure after firmware update

    We have an N9320B spectrum analyzer in our lab that had firmware B.02.52 on it. I've been controlling it via Linux 'usbtmc'. Multiple machines have used it, this one is debian with kernel 4.19. I decided to update the...
    buckd
    last modified by buckd
  • Keysight SAL Demo Code - How to increase the span above 20MHz?

    I've recently started with the SAL demo code to interface with the N6841A RF sensor and I wanted to know where in the code I would go to have the option of increasing the span above 20MHz to say a useful span of 40MHz...
    aj0994
    last modified by aj0994
  • product specific training

    I am  looking for a product specific training or workshop or demonstration for PXE N9048B. Please advise if any such resource exists. 
    balaji4799
    last modified by balaji4799
  • E4402A vsa 89600 software

    I have gor an E4402A,please could some tell if this A model supports vsa 89600 software?--i know that the B models are supported! Regards Hardy
    hardyhansen
    last modified by hardyhansen
  • Uncertainty measurement with GUM

    Hi everyone    I have a question about the measurement uncertainty. (Base on CTIA chapter 7) What is the meaning of the receiving device uncertainty? Is it the data on equipment datasheet ? If so, should...
    william_woo
    last modified by william_woo
  • Luminous suppression error when turning off the 8564E

    I have the wonderful spectrum analyzer 8564 E. Only when turning off the light spot is not suppressed. You see a roughly rectangular light field that fades in 1-2 seconds. What could I investigate for lack of circuit?
    magnetling
    last modified by magnetling
  • Can't upgrade N9010A from 23.13 to 25.05

    I have an N9010A running Windows 7 and XSA software version 23.13. When I try to upgrade the software to the current version (25.05) the instrument reads the installer software from the USB stick, but eventually hangs...
    swperk
    last modified by swperk