• Trace using Marker Noise

    I am using an E4443A Spectrum Analyser and interfacing with it via SCPI commands using MatLab. I am trying to get a trace from the instrument similarly to what is returned by the 'trace:data? trace1' SCPI command, but...
    rpash
    last modified by rpash
  • Option 049 license key of E4403B

    Hello Keysight team,  Please help to retrieve the option 049 license key of E4403B s/n : US 39150120. The display screen is only monochrome.   Thanks  
    moi
    created by moi
  • problema hp 8593e

    dopo che si è scaricata la batteria di backup, avendola cambiata con una nuova l'analizzatore mi da una rappresentazione della schermata principale cioe' uno scalino e non la classica visualizzazione facendo le...
    francesco001
    last modified by francesco001
  • ESA Series - Not correct Model Recognition A7A4 Assy

    I recently had to substitute the Processor Board (A4) from a E4404B SA. The original board did not boot anymore, tried by all means, no chance. After installing new board, SA works perfectly (performed complete automa...
    RudyMuller
    last modified by RudyMuller
  • ESA E4407B License Keys

    Hello. Restoring an E4407B (more on that later) but confused by the "installed" license keys. The preamp does NOT appear on the 'Amplitude' menu.   Can you tell me what keys should be available?   s/n =...
    MarkBielman
    last modified by MarkBielman
  • HP 8595E option 140 not listed after memory battery replacement and tracking generator

    Question 1 : I replaced the memory battery in my HP8595E and I lost the correction constant and options 105 and 140. I retrieved the correction constant from a backup and I did get back a fully functionning option 105...
    highroller
    last modified by highroller
  • Blown E4407B... bad RYTHM?

    I am repairing an E4407B at work (blown attenuator) but I think there is another issue. Look at this screen upon power up: The high noise floor should NOT be there. Drops at almost exactly 3 GHz. Suspect the RYTHM ...
    MarkBielman
    last modified by MarkBielman
  • Transmitting a CW or a modulated signal

    Hi All,   I transmitted a CW or a modulated signal at 60 GHz. The baseband signal was generated in arbitrary waveform generator and a VSG was used to upconvert the IQ inputs from the AWG at 5 GHz. To transmit at...
    mahfuza
    last modified by mahfuza
  • LTE DCI0 Decoding Issue on the N9020 MXA when Signal Playback from N5172B MXG

    Hi , I'm Trying to configure the N5172B MXG with a Configuration consisting of only DCI0 with NDI as 1 and TPC bits as "1" for a RNTI 65 with iMCS4 and NumPRB 4 for computing the RIV bits. This signal is generated and...
    satishvema
    last modified by satishvema
  • Personality Module

    Is there any option to configure the N9010B Signal Analyzer to behave the E444X series spectrum analyzer? The reasoning is that we have automated test code that only recognizes the E444X series and do not have a resou...
    freddayz
    created by freddayz
  • HP83640B OPTION H10

    HP83640B OPTION H10  WHAT IS OPTION H10?
    jlaguard
    last modified by jlaguard
  • ESA Hardware ID Codes

    Hello. Just picked up a used E4407B (needs help) and wondering what's up with the strange results on the hardware screen.    Not sure if HW ID 226 is real or not.   Anyone have a list of these ID co...
    MarkBielman
    last modified by MarkBielman
  • MXA- N9020A Signal Analyzer SCPI CMD Not working

    Hi ,   I am trying to use this SCPI command ":CALCulate:DATA?"  in Python but I am facing issue with ValueError: Could not find **** sign (#) indicating the start of the block.   Also If possible ca...
    dhanabal.kulan@hcl.com
    last modified by dhanabal.kulan@hcl.com
  • How do I revert my 8594E analyzer back to stock and un-install options 151/160 ?

    Picked up an 8594E relatively cheap (it works fine) but it doesn't have narrow RBW filter, FAST ADC (for analog + display capability) and AM/FM demod options. It came with the TG and option 119 (which is easy to remov...
    PeterM
    last modified by PeterM
  • E4402B, Dead battery caused licensing issue

    I have an old E4402B that hasn't been used for about a year and its internal battery died since it was last used.  I've replaced the battery and now it keeps time, the settings, and it knows its been aligned now ...
    MSchutzer
    last modified by MSchutzer
  • Noise power measurements on PSA series spectrum analyzers

    Hi,   We are using PSA series spectrum analyzers in our MMIC validation setup. I had the following question on the use of a noise marker.   I would like to measure the noise density(dBm/Hz). Would there b...
    nsm
    last modified by nsm
  • N9344C Frequency range

    We have "N9344C" spectrum analyzer and as per datasheet frequency range is 1MHz to 20 GHz. Can I use this spectrum analyzer for the input frequency of "100KHz to 1MHz"?
    Yashodip
    last modified by Yashodip
  • N9342C HSA Log Frequency Scale

    The HSA user guide says that using a log-frequency scale is useful for filter analysis: "When measuring filter characteristics, it is useful to look at the stimulus response over a wide frequency range. Setting the an...
    wreeve
    last modified by wreeve
  • Real Time RTSA and FFT

    Hi,   I have the following question with regards to real time. If I work with my N9020B in normal spectrum analyzer mode, I can either have the traditional swept mode or alternatively, I can move to FFT sweep to...
    batigol
    last modified by batigol
  • N9030A PXA Average Detector

    I currently am using a N9030A PXA and am getting varying differences in readings when I use Average Detector and EMI Average Detector. Can someone please explain the difference of these two setting to me.   Thanks
    nellints
    last modified by nellints