• How 89600 VSA decodes the MAC address

    Hi everybody,   I am monitoring the Wifi signal using WLAN 802.11a/b/g/j/p application. There are several wifi AP in the area that I have put the signal analyzer. 89600 VSA software is also installed and everyth...
    GeorgeMasonUniversity
    last modified by GeorgeMasonUniversity
  • User-defined Filter

    I use the analyzer N9010A. Tell me please about the User-defined Filter! I can not understand how to correctly set the impulse response in text form. The manual says that the trace should be in the time domain! Please...
    sniper53
    last modified by sniper53
  • E4406A license files

    As this analyzer is now out of support, is there any chance that you'd consider making license files for the options available?   Mine came with quite a few options (202, 204, BAF etc ...) but I'd quite like to ...
    perdrix
    last modified by perdrix
  • Capture Demodulated IQ samples

    Is there a way to capture the demodulated IQ samples. I had captured IQ MeasTime trace earlier but after post analysis on MATLAB it seems to be the input signal. The Syms/Errs table gives the hard decision bits, I wan...
    suchita
    last modified by suchita
  • Apply for educational VSA license

    Dear Keysight,   We already filled out the application form for the educational VSA license in March, but no response was received by us not by email and not by phone. So I decided to try to get some help via th...
    Csaba
    last modified by Csaba
  • We are facing the issue while installing the driver for the N9000A CXA Signal Analyser which is downloaded from the keysight website

    We have downloaded the driver for the N9000A CXA signal analyser from the keysight website and facing the installation issue.
    jeevan
    last modified by jeevan
  • What is the role of a 100 Ohm resistor between the input channel Ground and source channel Ground of FFT Analyzer 35670A?

    I am using Agilent 35670A (now is keysight 35670A). When I used it to measure the output voltage noise of my device, I found there is a lot of noise at frequency higher than 30kHz.   I was quite confused,...
    denghb
    last modified by denghb
  • Recreating the hard drive on an N9020A

    I just acquired an N9020A that is complete except that the hard drive is missing. All of the other hardware is present and appears to be in good condition. Based on the BIOS screen, I believe it has an older generatio...
    swperk
    last modified by swperk
  • Free 30-Day Trial Licenses for X-Series Measurement Applications for X-Series Modular Instruments

    Hi,   I just wanted to post a reminder that *FREE 30-Day Trial Licenses* for X-Series Measurement Applications for X-Series Modular Instruments are available via Keysight.com.   Link: 30-Day Free Tri...
    FrankC
    last modified by FrankC
  • 89600 Video Bandwidth (VBW)

    How/where is VBW controlled when using the 89600 spectrum analyzer software?  
    NavWorx
    last modified by NavWorx
  • Problem with 89601B custom OFDM measurements

    Hi,   We've been using the 89601b custom OFDM demodulation software for many years now and at some point along the way we have found cases where we are not getting accurate or meaningful I/Q imbalance measuremen...
    LLASCA_eesof
    last modified by LLASCA_eesof
  • How to order Transportable license?

    Hi, I want to order 89601B-200 (it has transportable license). According to our data, we have 2 way to purchase this application: 1- in this way, we should buy Signal Analyzer instrument (for example N9020) with ins...
    saeedgholami20
    last modified by saeedgholami20
  • Hi am using N9030A-526 spectrum analyzer and am using 2151-DK-0048 coax cable ,so how can i measure the insertion loss of this cable using spectrum analyzer...Thanks in advance

    Hi All, I am using N9030A-526(3Hz-26.5Ghz) spectrum analyser and am using a 2151-DK-004 coax cable, may I know how to measure the cable loss using N9030A spectrum analyser. Thanks in Advance
    kumar001
    last modified by kumar001
  • Cannot find RawDataValue/RawDataValueUnit properties in Trace object in COM API

    I am trying to use the COM API in LabVIEW running on the Infinium VSA80000A (basically, a DSO81204B scope with VSA SW).  I find the RawDataValueNames property, but there is no sign of the RawDataValue/RawDataValu...
    ushamsi
    last modified by ushamsi
  • Cannot find RawDataValue/RawDataValueUnit property in Trace object

    Using COM API in LabVIEW running on the Infinium VSA80000A (Basically, a DSO81204B scope with VSA SW).   I can see the RawDataValueNames property, but not the RawDataValue/RawDataValueUnit properties, though the...
    ushamsi
    last modified by ushamsi
  • 35670A DSA Calibration in progress

    Respected, I had a problem with 35670A DSA using for noise analysis, once after started the device it is booting and it was showing calibration in progress in mid of screen and the system is hanging no button is work...
    surya
    last modified by surya
  • 89600 VSA Frequently Asked Questions & Answers

    Here is a great starting point for answers to ~120 commonly asked 89600 Vector Signal Analyzer questions ....  Agilent 89600 VSA FAQs   Quick links to key FAQ categories include ....   Calibration &am...
    litzdog911
    last modified by litzdog911
  • Try out the full 89600 VSA software for 14-days, free ....

    You can order a CD with the full 89600 Vector Signal Analysis software, including all optional modulation formats and measurement hardware interfaces.  The free trial license provides full functionality for 14-da...
    litzdog911
    last modified by litzdog911
  • How do I measure Chirpped Pulse's SSL and PCR

    Maxim  Afanassiev, an Agilent Applications Engineer from Russia, wants to help a customer measure the quality of a linearly chirped pulse.  The quality metrics are Side Lobe Level (SSL) and Pulse Compression...
    bobmat
    last modified by bobmat
  • How can I program the 89600 VXI Hardware?

    Check out the information here regarding programming the 89600 VXI modules using COM and VISA-based programming tools .... view
    litzdog911
    last modified by litzdog911