• DSO-X 3012A randomly freezes during USB data transfer

    Hello everyone,   I'm having troubles with the Agilent DSO-X 3012A oscilloscope, firmware version 02.43.2018020635. I intend to use it to perform a series of measurements (hundreds of thousands), downloading eac...
    PetrSocha
    last modified by PetrSocha
  • Looking for a  user manual and probes for Lectrotech TO-55 scope

    Hello everyone, I found a Lectrotech TO-55 oscilloscope at a hamfest after it was over. It works, but there are no probes with it. And I don't have any information on the scope. So, I was hoping at the very least, th...
    patrickdickey52761
    last modified by patrickdickey52761
  • Hello Folks, oscillo DSOX2024A, suffering black screen after long inactivity (>1 year off). Suggestions?

    Oscilloscope stored in working conditions, and after long inactivity period denies to restart (Only black screen).   Internal visual inspection OK, all condensators OK, battery 3V OK, fan working, various power ...
    profesorcristobal
    last modified by profesorcristobal
  • I have an obsolete (but still very useful) HP 54201A. One of its self tests checks the input circuits. The service manual says to connect a BNC cable from the rear BNC to the input BNC on the front to perform the test. What sort of cable is it talking abo

    Thanks for any assistance. 
    psteichen
    last modified by psteichen
  • AgInfiniivision MATLAB driver commands

    In test and measurement tool, I am finding it difficult to use the commands in the 'scope-AgInfiniivision' Functions in MATLAB. Is there any support available where I can learn to use these commands through examples.?...
    MayankBrainAlive
    last modified by MayankBrainAlive
  • Delta Time Measurement Error

    I am using DSO90804A for some delta time measurements in the order of 50ps. The scope datasheet lists the measurement error limit in pg-26.    Is the error limit applicable only when sin(x)/x interpolation ...
    vinodh_cyp
    last modified by vinodh_cyp
  • How to attach a homemade probe to an AutoProbe socket ?

    How can I make a probe that attaches to the AutoProbe interface and gets properly detected (beyond simple resistor programming) ?   Is there a way to provide probe info for the S-Series scopes so that a homemade...
    Wolfgang
    last modified by Wolfgang
  • How get minimum analog input voltage for an oscilloscope DSO-X3024A?

    How can I find the minimum analog input voltage for an oscilloscope? I've checked the datasheet for the particular one I am using(Agilent DSO-X 3024A) and only the amplitude (maximum) voltage is listed.It would be bet...
    jr1972
    last modified by jr1972
  • Test the Signals of Wireless Vibration transmitter on oscilloscope

    I want to test the analog wave signal fo sensors which are connected with wireless mesh module just like the one connected with wireless vibration transmitters and also need to check the waveform on receiver end to te...
    varul29001
    last modified by varul29001
  • Digital Serial Analyzer Sampling Oscilloscope DSA8200

    I have NI measurement system  consist of two chassis VSA & VSG to generate and acquiring the signals. I have connected Oscilloscope DSA8200 to measure the time domain waveform and to check them with the ...
    A.E.D
    last modified by A.E.D
  • Wie ermittelt man automatisch die kleinste Amplitude? DSO-X 3024A

    Ich habe den DSO-X 3024A. Es bietet zur Messung von Amplituden eine Befehl: Typ: Ampl. an. Jedoch wird hier bei verschiedene Amplitudenformen dann das größte Signal. Es gibt keinen Befehl wo die kleinste Amp...
    jr1972
    last modified by jr1972
  • Measure Delay from Trigger?

    Hi: On a DSO-3000X, I'd like to measure the period of a clock signal with a high degree of time resolution.  This may be to determine jitter, or to characterise intermittent anomalies. So I configure a simple e...
    mr.crc
    last modified by mr.crc
  • I get error RTHDCPL.exe - Illegal system dll relocation!

    Yesterday, my scope was working fine and now I am getting the following error message: The system DLL user32.dll was relocated in memory. This application will not run properly.   The relocation occurred b...
    Forumsadmin
    last modified by Forumsadmin
  • HP 54616C rotary encoder erratic behavior

    I have issues with both of my 54616C oscilloscopes. The knobs for time and voltage (both channels) on both oscilloscopes generate unstable values when turning the knobs. Two clicks in the same direction may produce on...
    danish
    last modified by danish
  • IVI-C drivers for U2701A available?

    I am using KeysightU2701A U2701A Oscilloscope. Are there IVI-C drivers for U2701A available?
    Scope
    last modified by Scope
  • POWERLINK validation

    Good morning. I need to validate a POWERLINK connection, which is nothing more than a real-time ethernet protocol. In order to do this, I'd like to use my DSOS104A oscilloscope. I've seen this brochure https://li...
    andrea.miclausig
    last modified by andrea.miclausig
  • DSOX1102G FRAN, Move marker on results via programming (remote control).

    Hi all,   I have a python program, using visa, that controls a DSO1102G.  During this routine a frequency analysis (FRAN) section is run, and the results are displayed on the scope.  I can successfully...
    CKnudsen
    last modified by CKnudsen
  • MSOX2024A Snapshot (Wish List)

    It would be nice if in a future firmware update <hint, hint> for the 2000-X Series that you could screen capture the snapshot measurements screen. One screen capture with all of the available info needed in one ...
    ScopeDope
    last modified by ScopeDope
  • How to chose the right Bandwidth for a given Application

    We are working on a power electronic converters, where the switching frequncy is 1 MHz. However the transient might be at a frequency higher than the 1 MHz. What shd be the appropriate bandwidth for this application. ...
    lenin
    last modified by lenin
  • Issue by compensating probes. Signal goes down after few minutes.

    Hi all,   Few days ago I've got a HP/Agilent/Keysight 54610B, like this one below:     It works perfect but ... When I try to compensate my probes and after 5 minutes approx the square signal goes d...
    jaimebcn
    last modified by jaimebcn