Skip navigation
All Places > Discussion Forums

Oscilloscopes

Log in to follow, share, and participate in this community.

Recent Activity

malli1729
Hi, We need to measure power supply noise measurement for 0.82V,1.0V,1.2V,1.8V rails. Setup will be: 50Ω, RF176 Co-axial probe directly soldered across output capacitor, configure oscilloscope input to 50Ω and with lowest vertical division to measure the ripple. Low end scopes like DSOX3024A have offset ranges up to ±2V, but new scopes can't… (Show more)
in Oscilloscopes
Phung
We would like to upgrade the firmware on our UXR0051AP from 10.25.00902 to 10.25.01104. Please point me to a procedure for how to do that.   Thank you, David
in Oscilloscopes
aviad_meg
Hey, In my project I am sampling an analog signal in 1G sample rate using a digitizer function in the oscilloscope and with Labview I am writing the values that I gat from thus sampling into excel file using: My question is how to get the row data of thus values (in bits or Hexa, not an absolute number like I get now)?   kind regreds, from Aviad
in Oscilloscopes
GregWang
Hi,   I have been trying to make a simple waveform Acquisition LabView program with a rising edge trigger.   However, I kept getting 'Error Code :  -222  Error Message :  Data out of range', and I don't have a clue on how to resolve it.   I have attached a Snippet of my program along with the question. Please let me know if you spot anything… (Show more)
in Oscilloscopes
asatar
Click to view contentInfiniium SW Version: 06.55.00702   From debug log:   #trying a query  > :MARK1:CMOD?$ ?                           ^ ? -113, Undefined header > <NL+END> > ? ^ ? -420, Query UNTERMINATED     #trying a command > :MARKer1:CMODe SOUR$ ?                              ^ ? -113, Undefined header > <NL+END>   Using p.749 of programmer manual:
in Oscilloscopes
alberto_ugr
We have an old DSO3062A (Agilent 3000 series) at our lab, which I am trying to connect to a computer running windows10.  No matter what I do, the computer does not recognize the device, and the "Scope connect software" does not detect the oscilloscope - I get the error message "can't connect to usb device". Along with the oscilloscope comes a CD… (Show more)
in Oscilloscopes
humgar
I saw "Demo Clock" as one of the options in the Calibration window's Aux (Output) pulldown menu. It's a 456.35Mhz signal, but I've never seen any reference to it on the Service Manual or the User Guide. Out of curiosity, is there any purpose for the "Demo Clock" signal? Is it used in the self-calibration process? 
in Oscilloscopes
asatar
Edge-to-Edge measurements require Measure All Edges to be enabled. The documentation clearly states measurements will be made on all edges within the acquisition even those occurring off screen.    Is the way to ensure that the Edge-to-Edge measurement is only made on what's on screen setting the memory depth to correspond to the displayed… (Show more)
in Oscilloscopes
asatar
Click to view contentI have the following signal activity :   There are thousands of CS_n pulses that occur in a sequential one-shot fashion, and I'd like to be able to "stack" or "fold" them over a period of 5ns or so to make some measurements between CS_n and CLK.   Simply triggering on the falling CS_n edge does not accomplish this. The acquisition looks like… (Show more)
in Oscilloscopes
Eric003
I have a HP54645D with HPIB module HP54657. If I set a HPIB address eg. 13 this address is lost over 1 day, if I read the address back I get 10. From a prior post I learned that it is not unusual that in old RAMs or EEPROMs "stored data files could be corrupted" My questions: -- is the HPIB bus address also stored in NV-RAM (buffered by a… (Show more)
in Oscilloscopes
Load more items