• 4-port E5071C vs N5230A

    Hello,   I used 4-port E5071C to measure twisted-pair cables and differential channels on PCB. Basically, it can cover S-parameter measurements and provide .s4p file.   Now we need to purchase a VNA f...
    h4ttrang
    last modified by h4ttrang
  • N5230A - How to see in the smith chart impedance in module and phase?

    I can see resistance and capacitance but i cann´t measure in module and phase
    ICM
    last modified by ICM
  • Problem trying to set the correct loss (0.93 Gohm/s) for an 85054B type-N calibration kit on an 8753ES

    I'm trying to use an 85054B type-N calibration kit on a 3 GHz 8753ES with the latest (7.74) firmware. The 85054B is not in the 8753ES firmware - I'm guessing Agilent didn't think anyone would use such a very expensive...
    drkirkby
    last modified by drkirkby
  • Invalid power level in pulse profile

    Hello, I use N5242A PNA-X with FW 9.90.21. I am trying to perform pulse profile measurements according to the appnote "Active-Device Characterization in Pulsed Operation Using the PNA-X". I perform a frequency sweep ...
    stefek
    last modified by stefek
  • 8753E integrated vs. external test set

    I am working on a deal to upgrade my 8753C with 84074A 6 GHz test set to an 8753E.  I need to decide whether to keep the existing test set and get an option 011 analyzer, or get a unit with the integrated test se...
    JohnAckermann
    last modified by JohnAckermann
  • bitlocker

    Greetings, I was wondering if there were any known issues with enabling Bitocker on a Windows 10 PNA.  Here is a list of models that we currently use:   N5245A N5242A N9030A N5234A ENA 5063A
    Mario625
    last modified by Mario625
  • Can one convert a standard 8753D or later to option 014?

    The standard 8753D/E/ES have the built in test set. Option 011 removed the test set, which is less convenient, but more flexible.   I can’t quite recall what the very rare option 014 gives one, but it is a...
    drkirkby
    last modified by drkirkby
  • 8510C VNA softkey buttons cover.

    I'm trying to restore two 8510C VNA's (mine and a friend's) and I need two of the softkey buttons covers. The service manual says they are p.n. 08757-40012 but are NFS. Are there any other sources for them? Searc...
    SteveDBS
    last modified by SteveDBS
  • Device Measurement eXpert

    Open video

    daras
    last modified by daras
  • How to use a signal generator to trigger a single measurement? (PNA 5225A)

    Hello,   I am currently working on triggering a single measurement on the N5225A PNA with an external device. For the moment, I am just trying the trigger the measurement with a signal generator (sending square...
    cr85
    last modified by cr85
  • Lynx3dm tab missing

    Setting up a used PNA for external Monitor display the Lynx 3dm+ tab is missing. On the Keysight PNA and PNA-L Series of Network Analyzers, what are the hot keys to set-up the various internal and exte…  ...
    DavidC
    last modified by DavidC
  • Run Soft Front Panel hidden?

    We purchased Qty 3 P93XX network analyzers and they arrived yesterday. Now we have to write drivers for them. Most of the time, we anticipate that we will be using custom test software to communicate with the instrume...
    BillEaton
    last modified by BillEaton
  • HP 85047A test set coupler (5086-7489) - disassembly

    HP 85047A contains HP 5086-7489 test port coupler which grossly fails simple directivity test (terminate with known-good APC-7 50 ohm load, and almost all source drive signal appears on the coupled port save for a not...
    wb0gaz.
    last modified by wb0gaz.
  • Multi-site function support for M980xA

    The on-line help  Rev A.13.70 (M980xA/P500xA)   Rev A.13.10 (P937xA)   Rev A.12.60.xx (M9485A/M937xA) -  2-Jul-2019 states that the M980xA doesn't support the multi-site function. Is this...
    LOlson
    last modified by LOlson
  • Pinging Joel - something to amuze you.  / How would I measure the dynamic range of a VNA?

    I've splashed out recently on a new 2-port VNA. My budget would not quite stretch to a PNA-X, so had to make do with a NanoVNA which costs £50.99 (less than $65 USD) - luckily that included shipping!  I don'...
    drkirkby
    last modified by drkirkby
  • Is there anyway we can force to overwrite the cal to CHn_CalReg instead of appending. It looks like In E8364B, It is overwriting to CHn_CalReg whereas in N5225A it is appending.

    Hi All, I found from the N5225A manual and it says   New with PNA Release 5.0, Calibration Registers are designed to simplify calibrations for most users. When a calibration is complete, the data is automatically...
    sumang
    last modified by sumang
  • Is there anyway we can force to overwrite the cal to CHn_CalReg instead of appending. It looks like In E8364B, It is overwriting to CHn_CalReg whereas in N5225A it is appending.

    Hi All, I found from the N5225A manual and it says   New with PNA Release 5.0, Calibration Registers are designed to simplify calibrations for most users. When a calibration is complete, the data is automatically...
    sumang
    last modified by sumang
  • Turning off a VNA?

    I have an E5071C, and the standard method to turn if off is to press the white "Standby Switch" button on the lower-left corner on the front panel. If a user turns it off by going through the software process (the Win...
    hugorain73@gmail.com
    last modified by hugorain73@gmail.com
  • can 8753D be used to replace 4395A? I need to do cross talk inspection under 30KHz and 1MHz

    In the previous testing by using 4395A, a test set of transmission/reflection 87512A is placed.  any test set is required if using 8753D?  Thanks
    Yuri03071226
    last modified by Yuri03071226
  • Insensitive mouse cursor on the touch screen

    I have an E5071C. To touch-move the mouse cursor, I need to tap the desired position on the touch screen many times or even keep pressing that position for more than a second before the mouse can move there. Unplug an...
    hugorain73@gmail.com
    last modified by hugorain73@gmail.com