• Invalid power level in pulse profile

    Hello, I use N5242A PNA-X with FW 9.90.21. I am trying to perform pulse profile measurements according to the appnote "Active-Device Characterization in Pulsed Operation Using the PNA-X". I perform a frequency sweep ...
    stefek
    created by stefek
  • How to use a signal generator to trigger a single measurement? (PNA 5225A)

    Hello,   I am currently working on triggering a single measurement on the N5225A PNA with an external device. For the moment, I am just trying the trigger the measurement with a signal generator (sending square...
    cr85
    last modified by cr85
  • Lynx3dm tab missing

    Setting up a used PNA for external Monitor display the Lynx 3dm+ tab is missing. On the Keysight PNA and PNA-L Series of Network Analyzers, what are the hot keys to set-up the various internal and exte…  ...
    DavidC
    last modified by DavidC
  • Run Soft Front Panel hidden?

    We purchased Qty 3 P93XX network analyzers and they arrived yesterday. Now we have to write drivers for them. Most of the time, we anticipate that we will be using custom test software to communicate with the instrume...
    BillEaton
    last modified by BillEaton
  • HP 85047A test set coupler (5086-7489) - disassembly

    HP 85047A contains HP 5086-7489 test port coupler which grossly fails simple directivity test (terminate with known-good APC-7 50 ohm load, and almost all source drive signal appears on the coupled port save for a not...
    wb0gaz.
    last modified by wb0gaz.
  • Multi-site function support for M980xA

    The on-line help  Rev A.13.70 (M980xA/P500xA)   Rev A.13.10 (P937xA)   Rev A.12.60.xx (M9485A/M937xA) -  2-Jul-2019 states that the M980xA doesn't support the multi-site function. Is this...
    LOlson
    last modified by LOlson
  • bitlocker

    Greetings, I was wondering if there were any known issues with enabling Bitocker on a Windows 10 PNA.  Here is a list of models that we currently use:   N5245A N5242A N9030A N5234A ENA 5063A
    Mario625
    last modified by Mario625
  • Pinging Joel - something to amuze you.  / How would I measure the dynamic range of a VNA?

    I've splashed out recently on a new 2-port VNA. My budget would not quite stretch to a PNA-X, so had to make do with a NanoVNA which costs £50.99 (less than $65 USD) - luckily that included shipping!  I don'...
    drkirkby
    last modified by drkirkby
  • Is there anyway we can force to overwrite the cal to CHn_CalReg instead of appending. It looks like In E8364B, It is overwriting to CHn_CalReg whereas in N5225A it is appending.

    Hi All, I found from the N5225A manual and it says   New with PNA Release 5.0, Calibration Registers are designed to simplify calibrations for most users. When a calibration is complete, the data is automatically...
    sumang
    last modified by sumang
  • Is there anyway we can force to overwrite the cal to CHn_CalReg instead of appending. It looks like In E8364B, It is overwriting to CHn_CalReg whereas in N5225A it is appending.

    Hi All, I found from the N5225A manual and it says   New with PNA Release 5.0, Calibration Registers are designed to simplify calibrations for most users. When a calibration is complete, the data is automatically...
    sumang
    last modified by sumang
  • Turning off a VNA?

    I have an E5071C, and the standard method to turn if off is to press the white "Standby Switch" button on the lower-left corner on the front panel. If a user turns it off by going through the software process (the Win...
    hugorain73@gmail.com
    last modified by hugorain73@gmail.com
  • can 8753D be used to replace 4395A? I need to do cross talk inspection under 30KHz and 1MHz

    In the previous testing by using 4395A, a test set of transmission/reflection 87512A is placed.  any test set is required if using 8753D?  Thanks
    Yuri03071226
    last modified by Yuri03071226
  • Insensitive mouse cursor on the touch screen

    I have an E5071C. To touch-move the mouse cursor, I need to tap the desired position on the touch screen many times or even keep pressing that position for more than a second before the mouse can move there. Unplug an...
    hugorain73@gmail.com
    last modified by hugorain73@gmail.com
  • Does the 4396B support 85046A test sets with mechanical transfer switch?

    I have an older 85046A test set with the original logic board (85046-60001) and a mechanical transfer switch.  I was fine with this (I thought), but upon connecting it to my 4396B combination analyzer, the analyz...
    mark03
    last modified by mark03
  • P9375A VNA

    Can you please tell me how often should I calibrate the P9375A?
    cp
    last modified by cp
  • Where would you measure temperature inside a VNA?

    I know the FieldFoxes, and believe the PNA-Xs, have a temperature sensor(s) inside. Where are those sensor(s) located?   I have a small lab at home, and can't run the air conditioning 24/7, so its fairly obviou...
    drkirkby
    last modified by drkirkby
  • 8753 question - how can I save a file with a given name to the internal floppy drive?

    I wish to save the state of an 8753 to a floppy drive, with a name of my choosing - not FILE00, FILE01, using GPIB, but can't seem to work out what commands to use.   I can do this from the front panel by saving...
    drkirkby
    last modified by drkirkby
  • What equipment would be needed to determine an N load has a return loss >= 42 dB?

    I was having a discusssion with one of my lecturers from university. He is looking for loads with a return loss of at least 42 dB to 3.4 GHz. What (if any) Keysight equipment could be used to measure a load and verify...
    drkirkby
    last modified by drkirkby
  • Capturing Raw Trace Data in SMC (Scalar Mixer Converter) Mode

    So, I have a network analyzer (specifically the P9374A, but this question doesn't apply to just this model). Is there a SCPI command that lets me capture raw trace data in SMC mode, something like what Calc:...
    pikafu
    last modified by pikafu
  • HP8753D CPU Upgrade (option: 000)

    Hi   I would need to get firmware v7 on my HP8753D. This requires the new cpu board (08753-60272) to be installed. The board is quiet readily available on the used market, but I cannot find an installation manu...
    akellerm
    last modified by akellerm