Skip navigation
Log in to follow, share, and participate in this community.

Recent Activity

asatar
Click to view contentThis is the result of the eye scan on differential clock: I have to manually set the threshold  to (100mV). The software always warns about invalid threshold setting outside what it thinks a valid range is when I start a capture.
in Logic and Protocol Analyzers
AELP
Hi   I'm trying to connect to the logic analyzer using remote dekstop. My LA is running windows10. The problem I'm having is when connecting remotely the credentials don't work. I've created a local user and have enabled remote access for it but this doesn't work. I also own other Keysight equipment like spectrum analyzer and for that Keysight… (Show more)
in Logic and Protocol Analyzers