• Fixture ID

    Hello everyone, Is there a command in BT-Basic or a way to read the fixture ID wired by the fixture vendor ? This ID is the one used by the Autofile.   Thanks for the help.   Jean
    JeanCorriveau
    last modified by JeanCorriveau
  • i5000 unmuxed fixture running is required to migrate to Muxed sytem Series 3/5. Is there any recomended path to reduce the amount of re-wiring?

    Migrate fixture unmuxed(cards unmuxed) to muxed system(hibrid standard) 
    Profe
    last modified by Profe
  • Bead Probe Probes

    Is there a special probe that should be used with Bead Probe Technology?  
    Dennis_Dyer
    last modified by Dennis_Dyer
  • Fixture house recommendation?

    Can anyone recommend some fixture houses in India? Do you have a list of preferred fixture providers?  
    sunuplin
    last modified by sunuplin
  • How do I do a plotgen?

    How can I output a HPGL file of the fixture so that I can print it? There used to be a tool called plotgen. Where can I find it?  
    PeteCheng
    last modified by PeteCheng
  • CFT Top and Bottom Side Devices and Pins

    When using cad format translator, use the following commands to set the top and bottom devices. block file                  &#...
    dbailey
    last modified by dbailey
  • interface pin block hp44202P

    Do you know if the part number HP44202 interface pin  block is always produce by Agilent ?  
    agc
    last modified by agc
  • 3070 fixture consultant (windows)

    Any help will be appreciated: I have two customers, 1 in China and 1 in Tokyo. ICT test type is Agilent3070 for windows. 3070 tests done in Tokyo, then software and fixture brought to China. All compilations produce...
    edoga
    last modified by edoga
  • Looking for PADS cad.format file

    I'm looking for a PADS cad.format example file for the .asc file using CFT. Does anyone happen to have one?  
    darnold
    last modified by darnold
  • Fixture overflow error - best solutions.

    I'm in the process of fixture design for a pretty big board - component and node count, and have got an overflow error. Can anyone help in the steps to take to resolve the problem. Verify Fixture Type is OK. Verify ...
    iandailey
    last modified by iandailey
  • COLORED WIRING

    I am trying to use 6 different colors for my fixture wiring(3070 unix) and I have a little idea about the set-up. I know that you have to modify the .hp3070 for this but I do not know the proper syntax. Anyone who s...
    edoga
    last modified by edoga
  • How to connect BNC to fixture

    Hi All, i have a problem with a test setup i am using. I have a diecast box that contains a PCB with the DUT mounted inside it. I am measuring leakage current with a power supply and electrometer. The problem i have...
    andrew257
    last modified by andrew257
  • SJ50 AOI .dat file

    Hello, Excuse me if I put my topic to bad place. We use SJ50 serie AOIs. I made a program which watches the .dat file and if an algorithm changes then my program makes a log file from the parameters of the modificati...
    nkohler
    last modified by nkohler
  • Wire wrap bits for 3070 P-Pins?

    I am looking for the “special” Agilent wire wrap bits that are necessary to wire the Agilent 3070 personality pins.  Specifically the 28 and 26 AWG bits. In the Agilent technologies 3070 Family Build...
    gdunn
    last modified by gdunn
  • SJ50 II AOI

    Hello, We use SJ50 II AOIs. Somebody knows it which one the last GUI version, that is useful to this series? Which version you recommend and where I can download it? We use Windows 2000 on AOI PCs but we would like t...
    nkohler
    last modified by nkohler
  • Preserving a test fixture

    Hello- I have a simple question. If I already have a fixture built and want to re-use it when the board spins, which 3070 file do I send to the layout engineer so that they do not move any existing testpoint locatio...
    visanic
    last modified by visanic
  • board_xy.o object file is corrupt(HFS 341)

    Hi ALL, I have a problem when do “fix cons” to generate the fixture file, system can’t load the fixture due to placement error : see => fix_cons_error.jpg says “board_xy.o” corrupt,...
    bin
    last modified by bin
  • probing on smd pad's?

    Hi, I have this board, that has smd on the bottom side (the first time i see this here). Now 6 nodes are inaccessible unless i probe on smd pads (resistors). Is this a good idea, who has done this?. Regards, Andre...
    ANDREL
    last modified by ANDREL
  • Testsight Plot Generator

    Hi, is anyone how use Plot Generator from Testsight to preview fixture data? thanks sepp  
    jreichmuth
    last modified by jreichmuth
  • Survey: Special fixture requirements for Boundary Scan?

    Hi all, How's everybody doing? I would like to poll everybody's experience in the testing of boundary scan using the 3070 generated boundary scan tests. Do you need to have any special fixture requirements? What are...
    adrianc
    last modified by adrianc