• SnapShottoData not working as expected

    I created a Matlab script that creates a histogram variable "Counts" depending on which path and measurement I want to analyze from corresponding MonteCarlo datasets.  "Counts" contains the bin values (specified ...
    tgroovy
    last modified by tgroovy
  • SiPro Differential S-Parameter Plots

    Hi, Have imported a simple flex ribbon cable Allegro layout into SiPro which worked fine.  Setup all of the ports and finished the simulation which completed and converged without any warnings or errors. Went t...
    CT_ALFA001
    last modified by CT_ALFA001
  • Failed to write LTD file to Disk

    Hello,   While simulating in SipiPro we are encountering below error,How can i resolve it?   "Error:Error:Fails to write LTD file to disk"    Also attached error image for your reference.
    Shravan001
    last modified by Shravan001
  • Optimizer's strange behaviour

    Hi, i've got strange bug during optimization in ADS.   I've make schematic based on few SnP files and AMI model of FPGA Tx and Rx to perform SI analysis and optimize transciever parameters. So i've specify Tx an...
    rf_dev
    last modified by rf_dev
  • ADS 2017 envelope simulation error

    I am simulating a Power amplifier design and my input is an envelope modulated signal with a sampling frequency 92.16 MHz. while using envelope simulation the "TIme Step too small" error is coming.  And it is tak...
    nk07
    last modified by nk07
  • Ideal Frequency Multipliers in ads

    Hello, I need to know how to fill the ideal frequency multiplier data based on the datasheet. I will be grateful if you could let me know for this specific component. (My mixer is RMK-5-571+ mini-circuit)
    parisa91
    last modified by parisa91
  • How to set the width of a rectangle as a tuneable parameter

    I have the gerbers for a PCB antenna, which I have imported into a Genesys layout. Changing the length of the antenna element changes the antenna's resonant frequency. How do I get Genesys to tell me how long it has t...
    adamgulyas
    created by adamgulyas
  • S parametre fitting

    Hi, all I have a problem that how to extract the circuits from microstrip in Fig1? I have measured the S parametre of the microstrip as a 2-port network and then how to fit the measured S_parametre by extracted circ...
    liuxin
    last modified by liuxin
  • Problem importing this PSPICE model

    Whenever I import this (http://epc-co.com/epc/documents/spice-files/PSPICE/EPC2036_V100_PSPICE.net): ----- ----- ----- * (C) Copyright Efficient Power Conversion Corporation. All rights reserved. *************...
    ren_zokuken01
    last modified by ren_zokuken01
  • Creating Custom Simulator Functions in ADS

    Right now I have an ADS workspace with parts, where I have measured SNP data files for each part's serial number.   In a s-parameter simulation I can perform a paramsweep over an array that lists all the se...
    tp78
    last modified by tp78
  • Issues with SIPro

    Tried to run the sample program of the Panda_Board layout using DC IR Drop analysis.  Did exactly what the online video asked, but get an error with the following dialog:   Starting PI-DC simulation.The comm...
    CT_ALFA001
    last modified by CT_ALFA001
  • Problem with the number of phase fronts when attempting to generate OAM

    Problem with the number of phase fronts when attempting to generate OAM: In brief, an OAM (Orbital Angular Momentum) beam with a specific mode l should present exactly l number of helical phase fronts in its radiatio...
    Harry.L
    created by Harry.L
  • IBIS-AMI Model Generation Error in SystemVue

    HI, I am try to generate the IBIS-AMI model using SystemVue W1714EP AMI Modeling Kit. I have Visual Studio 2015 update 3 installed in my laptop.   It gives the below error.   Please find below the e...
    robingupta91
    last modified by robingupta91
  • How to use LTD substrate file in ADS ?

    I want to simulate Transmission line in ADS momentum for that I'm trying to use substrate ,which I got from technology library(65nm TSMC) as a LTD file which I'm able to import in ADS momentum "substrate editor" but I...
    anteshoc
    last modified by anteshoc
  • DAta access component - change file during sweep

    I run a sweep optimization, and every time I am reading the circuit parameters from DAC (data access component). I want the current simulation generate the parameter files for the next sweep. So, I need to write the ...
    nukihs
    last modified by nukihs
  • Crashing ADS 2011.10 leads to 'locked' schematics/layout files

    This has happened a few times. I'll crash ADS and then reload it to try accessing the layout/schematic I was working on and I'll get the following error: http://imgur.com/D1PEXva This makes the layout/schematic in...
    jimmydean
    last modified by jimmydean
  • open .7zads

    I'm using 2019 ads. I need to open .7zads. Can you please help me to open it? I have attached the file herewith .
    Thisara
    last modified by Thisara
  • Is it possible to get loss parameters(RLGC) of transmission line in ADS Momentum ?

    I have created layout a for transmission line using commercial IC technology PDK  and performed sp simulation in ADS.Is it possible to get loss parameters(RLGC) of the transmission line in ADS so t...
    anteshoc
    last modified by anteshoc
  • Is there a random function in ADS?

    Hi, everyone. Is there a random function in ADS? I want to produce a signal with random initial phase. Thank you.   Best regards,
    SandyGao
    last modified by SandyGao
  • Can I create a LTE Systemvue project with only one UE, resource allocation type 1. The result CRC pass in VSA decode

    Hi Specialist,   I come from Vinsmart Company. I'm trying to use Systemvue to create the Reference Testvector for my RRH in LTE Project.   So I create a project having only one UE, resource allocation type...
    thangtv8
    last modified by thangtv8