• SnapShottoData not working as expected

    I created a Matlab script that creates a histogram variable "Counts" depending on which path and measurement I want to analyze from corresponding MonteCarlo datasets.  "Counts" contains the bin values (specified ...
    tgroovy
    last modified by tgroovy
  • Failed to write LTD file to Disk

    Hello,   While simulating in SipiPro we are encountering below error,How can i resolve it?   "Error:Error:Fails to write LTD file to disk"    Also attached error image for your reference.
    Shravan001
    last modified by Shravan001
  • IBIS-AMI Model Generation Error in SystemVue

    HI, I am try to generate the IBIS-AMI model using SystemVue W1714EP AMI Modeling Kit. I have Visual Studio 2015 update 3 installed in my laptop.   It gives the below error.   Please find below the e...
    robingupta91
    last modified by robingupta91
  • Can I create a LTE Systemvue project with only one UE, resource allocation type 1. The result CRC pass in VSA decode

    Hi Specialist,   I come from Vinsmart Company. I'm trying to use Systemvue to create the Reference Testvector for my RRH in LTE Project.   So I create a project having only one UE, resource allocation type...
    thangtv8
    last modified by thangtv8
  • How much it cost a ADS license

    Hi im interested to adquired a ADS License but i wanna know how much it cost for a studen   somebody can help me?  
    ArathAmavizca
    last modified by ArathAmavizca
  • How much it cost a studen license

    Hi i want to know how much it cost a studen license , and the type of support that give a student
    arathamavizcaib
    last modified by arathamavizcaib
  • RFAMP as LNA in SystemVue

    I am using RFAMP component from 'RF Design Library' in system vue. I want to define this amplifier as low noise amplifier (LNA) by defining its s-parameter values and noise figure at operating frequency.   But n...
    engrvip
    last modified by engrvip
  • DVBS2_FrameSync in DVB receiver

    Hi,   I’m working on DVBS2 receiver with SystemVue. In the library there is a block called „DVBS2_FrameSync“. Please refer attachment for description of it. My question is, I can’t find ...
    Owen002
    last modified by Owen002
  • Hi, We are using W1714EP (AMI Modeling Kit)

    Hi, We use it to generate IBIS-AMI models. We run equalization adaptation in our IBIS-AMI model and would need to know a way so that we can write the final adapted values in a log file etc. Is there any block/mod...
    robingupta91
    last modified by robingupta91
  • How in SystemVue the two thermal noise floor adds up after a combiner?

    I am making a Tx chain using IQ mixer, so the signal first passes through Hybrid-90 and then IQ mixer and they are combined (as shown in Figure below). The combiner at the output doesn't have any phase difference (i.e...
    Ifrah
    last modified by Ifrah
  • two questions to the DVBS2 library in SystemVue

    Hi,   I have two questions to the DVBS2 library in SystemVue.   There are CRCEncoder and BBScrambler blocks for transmitter but no corresponded counterparts for receiver. How to perform such tasks? The DV...
    Owen002
    last modified by Owen002
  • Hi, We are using W1714EP (AMI Modeling Kit)

    We use it to generate IBIS-AMI models. We have a flow that can generate .DLL files for windows but we cannot yet figure out how to generate the *.so files for linux using the flow . Can you please guide us what setup ...
    robingupta91
    last modified by robingupta91
  • SystemVue Phased Array Beam Pattern

    Hi,  How can I select the beam pattern and its settings in the results section after I have put together a simple Rx array chain?    Thanks
    AAmiriUK
    created by AAmiriUK
  • RF to Digital Simulation

    I want to use SystemVue or ADS to model and simulate a microwave receiver front-end. I want to simulate from RF input through the A to D conversion and generate digital I/Q signals for analysis. Can anyone point me to...
    gmsgator
    last modified by gmsgator
  • Radar example in SystemVue fails

    Hi,   I just ran the example simulation PD_Radar but an error occured:   Sdata ‚PD_Radar__Ant__S1‘: DataFileName provided „...\AntSData_new.s2p“ is not a valid file.   Can ...
    Owen002
    last modified by Owen002
  • FPGA programming and Hardware in Loop validation with custom firmware and chipset

    Hello, I need to program my FPGA+Antenna module pair, working as massive mimo with custom "Software defined radio" firmware. Is it possible to load it in fpga block in systemvue, and program my modules over...
    Rasik
    created by Rasik
  • SystemVue tool crash

    Hello Sir,            I am trying to debug an issue using systemVue and I am unable to get the solution of it.     Issue : For all this time I was simulating file with...
    Ravikiran
    last modified by Ravikiran
  • SystemVue simulation

    I encountered such a problem in the simulation process:"Failed to allocate memory during initialization",I hope experienced experts can guide me to solve the problem,thanks
    蓝色的眼睛盒
    last modified by 蓝色的眼睛盒
  • How can I combine a LTE and CW signal, and then download to M9381A using M9381A_Signal_Downloader

    As the subject, I'm trying to combine a LTE signal and CW signal using Combiner in SystemVue, and then Download to M9381A using M9381A Signal Downloader.
    NGUYENQuangTuan
    created by NGUYENQuangTuan
  • How do you feed table data into Amplifier_M@data flow models?

    I have a file of losses in a feed network generated within Genesys. I now want to use this file to assign appropriate losses to a 2x4 array of antennas. I see in one of the examples that they do something like this to...
    etroy
    last modified by etroy